This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564C: 26M crystal recommend

Part Number: CC2564C

Hi,

NX2016SA-26MHZ-STD-CZS-2.pdf

Attach 26MHz crystal datasheet. The frequency tolerance (±25ppm) is slightly over the datasheet required(20ppm). 

Due to my customer has produced PCB board, is there any other parts recommended with same package? Thanks a lot.

  • Hi Daniel,

    The CC2564CX can accommodate 2 XTAL frequencies, 26MHz and 38.4MHz.

    For the 38.4MHZ XTAL we recommend: TXC and the part number is 8Z38400009.
    For the 26MHz XTAL we recommend: NX2016SA (EXS00A-CS06025) or TST - TZ1325D. Note that this one is a -20 to 70C XTAL.

    I think the EXS00A-CS06025 may be a good option, but otherwise I do not know of any direct footprint replaceable ones.

    Thanks,
    Riz