Part Number: CC2642R
Hi,
With regards to "Advisory Sys_01" mentioned in the latest errata, it is bit difficult to understand
the exact scenario on how this errata will occur.
1.It is mentioned that "noise on the JTAG TCK pin", does it mean it occurs only during debug mode?
or is it during normal operation?
2.It also mentions about the below case.
"The input buffer controlled by IOC.IOCFGn.IE is enabled and the DIO input value is
the same level as the CCFG bootloader pin level (BL_LEVEL) when entering
Shutdown (GPIO input values are latched when entering Shutdown)"
-> DIO here means any GPIO pins or is it the only pin defined in BL_PIN_NUMBER ?
Please let me know if there is any example use case to understand how this errata could occur.
Best Regards
paddu