Part Number: CC2640R2F
Hi all,
I try to add HID profile into our application. First, I add HID profile into simple_peripheral and it work(device can pair, bond and receive HID code). Second, I add HID profile into simple_peripheral_oad_offchip but it cannot work.(device cannot pair with cell phone. The reason is 0x08, sniffer is showing below) I do the same step on both project. I don't know why the oad project cannot work, please give me some suggestions Thank you.
HW : CC2640R2 LaunchPad
SW : simplelink_cc2640r2_sdk_2_30_00_28 --> simple_peripheral/simple_peripheral_oad_offchip
I change some parameters
OSAL_MAX_NUM_PROXY_TASKS 2
to
OSAL_MAX_NUM_PROXY_TASKS 3
and
ICALL_MAX_NUM_TASKS 3
to
ICALL_MAX_NUM_TASKS 4