Part Number: CC2564MODA
Tool/software: Code Composer Studio
Sir, thanks for replying.
The spple demo code is working when I tried with command calls as they mentioned in link which you have sent. Now I tried to modify the code as my requirement that is in one board I configured as server , registered the spple service,and advertisingle which is working.And in another board I configured as client and connectle which is working so when I have tried to configured as discoverspple it is showing as error which means it is showing as no device information but this function when I tried with command calls it is working but it is not working when I tried to change through API calls so can you tell me Do I need to change anything for this function in program.