Part Number: SIMPLELINK-CC26X2-SDK
Tool/software: TI-RTOS
Hello Ti Experts,
I am trying to implement the SDFatFS module ____
I was following the example implementation detailed in the following link:
From that link I developed the following code:
#if FATFS_ON
#include "ff.h"
//#include "ff.c"
#include "SDFatFS.h"
#include <ti/drivers/SD.h>
/* Drive number used for FatFs */
#define SD_DRIVE_NUM 0
char fileName[100] = "1";
#endif
void mainThread()
{
#if FATFS_ON
SDFatFS_Handle sdfatfsHandle;
FILE *src;
// const char inputfile[] = "fat:"STR(SD_DRIVE_NUM)":input.txt";
/* Mount and register the SD Card */
sdfatfsHandle = SDFatFS_open(Board_SD0, SD_DRIVE_NUM);
/* Open the source file */
src = fopen(fileName, "r");
#endif
}
int main()
{
/* Call driver init functions */
Board_initGeneral();
I2C_init();
SPI_init();
UART_init();
#if FATFS_ON
SDFatFS_init();
#endif
// Declare task param structure and task handle
Task_Params taskParams;
Task_Handle sampleSensors;
Error_Block eb;
Error_init(&eb);
/* Create 1 task with priority 1 */
Task_Params_init(&taskParams);
taskParams.stackSize = 2048;
taskParams.priority = 1;
sampleSensors = Task_create((Task_FuncPtr)mainThread, &taskParams, &eb);
if (sampleSensors == NULL) {
System_abort("Task create failed");
}
//call BIOS_start() enables interrupts and starts the scheduler with BIOS
BIOS_start();
return (0);
}
I was having a number of issues with undefined symbols so I needed up directly importing ff.h and SDFatFS.c/h into the project. This brought the number of undefines down to the following:
undefined first referenced symbol in file --------- ---------------- SDFatFS_config ./SDFatFS.obj SDFatFS_count ./SDFatFS.obj ff_cre_syncobj ./ff.obj ff_del_syncobj ./ff.obj ff_rel_grant ./ff.obj ff_req_grant ./ff.obj
Any ideas on how to deal with these undefined symbols?
Also, I get a warning saying that the handle for the FATfs is not being used despite having it set equal to SDFatFS_open(Board_SD0, SD_DRIVE_NUM).
Any help would be greatly appreciated,
Thanks