This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC26X2-SDK: How do I tell if my CC26x2 sample is PG 1.1 ot PG 2.0

Part Number: SIMPLELINK-CC26X2-SDK

Hi,

With the release of the latest SDK in supporting all CC26x2 devices with a PG of 2.0, how can I tell physcially what PG revision is the sample from?

Understand that SDK supports the following SimpleLink CC13x2 and CC26x2 wireless MCUs with silicon revision E (PG 2.1), is 'E' marked on the silicon as part of the body marking?

Thanks,

Christina

  • You have to connect the board with the device to Flash PRogrammer 2 or Smart RF Studio to read the version. If you order a new CC13x2/ CC26x2 LP today (R, not P) you should get rev E. The material that is in the field today should be rev C.