Other Parts Discussed in Thread: CC2541, CC2640R2F, CC2640
hey
I would like to do some project .
Receiving data from one BLE device and transmit to another BLE device, Since BLE device cannot connect to multiple devices at a time.So we can go for two options
1. we have to go for Zigbee or thread for such mesh networking where i am not interested in learning new stack right now since i am much familiar with BLE.
2. Use an intermediate processor between two BLE devices by using BLE devices as booster packs for processor.
The reason why i am using two BLE networks because i have to do some operations on received data(like displaying, making sound etc.) and well as to transmit new data from that point.
which one of above two will be easier way for my project? If not is there any other way to do? If 2 is the option which processor is suitable for it. It should consume less power and less cost. The BLE device i am using is CC2541 ibeacon module.
Thanking You
Sumanth