Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: CC2640R2F
Tool/software: Code Composer Studio
Hello,
I am evaluating CC2640R2F SDK 2.40 in HCI mode.The goal is to use the example host test in (examples\rtos\CC2640R2_LAUNCHXL\ble5stack\host_test) to configured the CCR640R2F as extended scanner.
I am using the serial library of Python to send GAP commands and receive GAP events.
Plesae found the folowing configuration used:
2019-01-30 13:20:42,566 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x1D, 0xFC, 0x01, 0x00]
Opcode = 0xFC1D (HCIExt_ResetSystemCmd)
Parameter Total Length = 0x1
Type = 0x0
2019-01-30 13:20:42,572 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x05, 0x1D, 0x04, 0x00, 0x1D, 0xFC]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x5
Subevent_Code = 0x41D (HCIExt_ResetSystemCmdDone)
Status = 0x0
CmdOpCode = 0xFC1D
2019-01-30 13:20:42,572 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x00, 0xFE, 0x08, 0x08, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00]
Opcode = 0xFE00 (GAP_DeviceInit)
Parameter Total Length = 0x8
profileRole = 0x8
addrMode = 0x0
ramdomAddr = 0x0
2019-01-30 13:20:42,579 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x06, 0x7F, 0x06, 0x00, 0x00, 0xFE, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x6
Subevent_Code = 0x67F (GAP_HCI_ExtentionCommandStatus)
Status = 0x0 (Success)
OpCode = 0xFE00
DataLength = 0x0
2019-01-30 13:20:42,589 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x2C, 0x00, 0x06, 0x00, 0xCF, 0xF6, 0x69, 0x22, 0x91, 0xB0, 0xFF, 0x00, 0x05, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x0F, 0x93, 0x31, 0x81, 0x12, 0x0A, 0xEF, 0x13, 0x03, 0x2A, 0x52, 0x80, 0x0E, 0x6D, 0x59, 0xC9]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x2C
Subevent_Code = 0x600 (GAP_DeviceInitDone)
Status = 0x0 (Success)
DevAddr = 0xB0912269F6CF
DataPktLen = 0xFF
NumDataPkts = 0x5
IRK = [0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0, 0x0] [0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0]
CSRK = [0xF, 0x93, 0x31, 0x81, 0x12, 0xA, 0xEF, 0x13, 0x3, 0x2A, 0x52, 0x80, 0xE, 0x6D, 0x59, 0xC9] [15, 147, 49, 129, 18, 10, 239, 19, 3, 42, 82, 128, 14, 109, 89, 201]
2019-01-30 13:20:42,591 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x57, 0xFE, 0x04, 0x00, 0x00, 0xC3, 0x00]
Opcode = 0xFE57 (GapScan_setEventMask)
Parameter Total Length = 0x4
eventMask = 0xC30000
2019-01-30 13:20:42,595 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x06, 0x7F, 0x06, 0x00, 0x57, 0xFE, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x6
Subevent_Code = 0x67F (GAP_HCI_ExtentionCommandStatus)
Status = 0x0 (Success)
OpCode = 0xFE57
DataLength = 0x0
2019-01-30 13:20:42,598 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x55, 0xFE, 0x02, 0x06, 0x00]
Opcode = 0xFE55 (GapScan_setParam)
Parameter Total Length = 0x2
scanParamId = 0x6 (DuplicateFilter)
DuplicateFilter = 0x0
2019-01-30 13:20:42,602 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x06, 0x7F, 0x06, 0x00, 0x55, 0xFE, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x6
Subevent_Code = 0x67F (GAP_HCI_ExtentionCommandStatus)
Status = 0x0 (Success)
OpCode = 0xFE55
DataLength = 0x0
2019-01-30 13:20:42,604 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x53, 0xFE, 0x06, 0x01, 0x00, 0x20, 0x03, 0x20, 0x03]
Opcode = 0xFE53 (GapScan_setPhyParams)
Parameter Total Length = 0x6
primPhy = 0x1
scan_type = 0x0
interval = 0x320
window = 0x320
2019-01-30 13:20:42,608 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x06, 0x7F, 0x06, 0x00, 0x53, 0xFE, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x6
Subevent_Code = 0x67F (GAP_HCI_ExtentionCommandStatus)
Status = 0x0 (Success)
OpCode = 0xFE53
DataLength = 0x0
2019-01-30 13:20:42,609 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x51, 0xFE, 0x06, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00]
Opcode = 0xFE51 (GapScan_enable)
Parameter Total Length = 0x6
period = 0x0
duration = 0x0
max_number_of_records = 0x0
2019-01-30 13:20:42,617 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x06, 0x7F, 0x06, 0x00, 0x51, 0xFE, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x6
Subevent_Code = 0x67F (GAP_HCI_ExtentionCommandStatus)
Status = 0x0 (Success)
OpCode = 0xFE51
DataLength = 0x0
2019-01-30 13:20:42,622 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x07, 0x13, 0x06, 0x00, 0x00, 0x00, 0x01, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x7
Subevent_Code = 0x613 (GAP_AdvertiserScannerEvent)
Status = 0x0
event = 0x10000
2019-01-30 13:21:43,762 :: -------------------------------------------------------------------------------
@ TED command
raw = [0x01, 0x52, 0xFE, 0x00]
Opcode = 0xFE52 (GapScan_disable)
Parameter Total Length = 0x0
2019-01-30 13:21:43,766 :: -------------------------------------------------------------------------------
@ TED event
raw = [0x04, 0xFF, 0x06, 0x7F, 0x06, 0x12, 0x52, 0xFE, 0x00]
Event Code = 0xFF (HCI_VENDOR)
Parameter Total Length = 0x6
Subevent_Code = 0x67F (GAP_HCI_ExtentionCommandStatus)
Status = 0x12 (Invalid HCI Command Parameters)
OpCode = 0xFE52
DataLength = 0x0
The issue that during 1 minute no GAP_Advertiser/Scanner_Event recived with type "GAP_EVT_ADV_REPORT" even if the sniffer show ADV packets in the air.
I am missing something?