This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC26X2R1: Project Zero fails to come up

Part Number: LAUNCHXL-CC26X2R1


Tool/software: Code Composer Studio

We have 6 Launchpad dev boards, Four ordered 2 months ago, and 2 more just ordered and received

The revs of the boards received earlier (QTY: 4) are 

BOARD Label                            Processor

Rev 1.0 WCS037A                     CC2642 R1F C TI XJ9J P7CK G4

The revs of the boards just received (QTY 2) are 

BOARD Label                            Processor

Rev B WCS037                         CC2642 R1F E TI X8AJ P3QJ G4

In both cases the SDK is simplelink_cc26x2_sdk_2_30_00_34, and CCS is version CCS8.3.0.00009_win32

We have done all the updates suggested during installation and initial project loads on 3 separate Win10 machines 

Off the box the new devices appear as "Project Zero" in a network scan. The problem starts with the new units (Rev B boards) as the Project Zero is built under CCS, and then after building and linking, this message appears

After performing the upgrade successfully the CC2652 is no longer operational:

Our current status is that we have one board "down" as shown above. We did NOT and will not perform the upgrade on the second one. This board under power is still seen as a Project Zero device... 

=================

More related facts.

Of the four initial  (Rev 1.0) boards:

- 2 have been "killed" by the same forced upgrade

- 2 did not exhibit this issue. We do not recall whether a firmware update was forced  (we rather think not!!!!) and these boards now run both Project Zero and our own software successfully but with a twist:

--- one runs both connected to the host under the debugger and in stand-alone as a release build

--- one runs ONLY connected and in debug mode, NOT stand-alone.

Rev levels are identical, sofware loaded is exactly the same, but their behaviours are different.

=================

Questions:

[1] How does the forced debug probe update work and why does it put the CC2652 in this error mode? Is there a way to bypass making this upgrade? Or is there an incompatibility between this debug probe and the latest CCS updates? Or???

[2] Of the 6 boards received in total, why do 4 need this update, and 2 did not?

[3] Any idea why, in the 2 older boards we have that passed the initial stage, one only will work in released mode, and one not?

Our development work is stalled.. Thanks for any help or insight you may have.

  • I reviewed the post "CC13x2, CC26x2 Revision E and SDK version compatibility" and this looked like the problem would be the SDK incompatibility listed there: Rev C silicon with 2.30... SDK and Rev E silicon with 2.40...SDK
    Unfortunately this may be part of, but not the whole solution.

    Our first 4 launchpads are rev C silicon and we used 2.30 SDK. As mentioned above, 2 come up, and 2 don't
    Additionally our latest 2 launchpads are rev E silicon, and we used the 2.40. SDK for those
    - the one we had done the upgrade on loads Project Zero without error but does not come up as a BLE device
    - the one we haven't touched asks for the upgrade. Image I inserted isn't displayed .Message is
    ........."Warning:
    A firmware update is required for the debug probe. Click the "Update" button to update the firmware and connect to the debug target.
    DO NOT UNPLUG THE DEBUG PROBE DURING THE UPDATE.
    (Emulation package 8.0.903.6)"............. I did NOT proceed......
  • Hi Sylvain,

    The error message images in your post are broken.

    1) The debug update updates the firmware on the XDS110 on the LaunchPad. I have not heard of this causing an error mode. However, there is a known issue where, after a debug probe firmware update, CCS can not connect to the device. This is solved by pressing cancel, then press the debug button. (Now CCS will successfully connect to the device.)

    2) This will depend on the firmware on the XDS110 compared to the CCS version

    3) Sounds like you were not able to program this device successfully.

    Please do the firmware update when asked.

    Can you try following the steps in this SimpleLink Academy lab to program Project Zero on the devices: dev.ti.com/.../