Other Parts Discussed in Thread: UNIFLASH
I have a few questions regarding the CC2640R2F
- Why is there a voltage level translator (SN74AVC4T245RSV) between the XDS110 and the CC2640R2F?
- To program the image using Uniflash is the only requirement UART TX and RX pins?
- To flash the image, is there any other pin (SOP pins etc.) needed to boot the device in flashing mode or that is not applicable to the device
- The mmWave EVM being designed will interface with the BLE device using SPI and UART, are there any other pins/interface needed to connect the CC2640R2 to a host/slave MCU
- The only XDS110 interface to the BT will be the UART RX and TX, is this sufficient?
Regards,
Charles O