Part Number: SIMPLELINK-CC26X2-SDK
Tool/software: TI-RTOS
We want to develop our own applications based on the project(simple_peripheral/project_zero).
Regarding the simple_peripheral project, it has the following configuration....
// Enable iCache prefetching
VIMSConfigure(VIMS_BASE, TRUE, TRUE);
// Enable cache
VIMSModeSet(VIMS_BASE, VIMS_MODE_ENABLED);
However, the project_zero project doesn't have these configurations.
Do we need to copy the above configuration into the project_zero project?
Could you also help to provide some description on the above configuration?
If the above configuration will affect performance, is simple_peripheral project more efficient than project_zero project?????