A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC2652R: Do we have an updated BLE Mesh status of our SW as Post in e2e is from 2017?
There is no update as of now. BLE Mesh is still in an early stage and a very simple mesh solution. We recommend using more mature mesh protocols with better performance such as Zigbee and Thread, or alternatively consider a star network running sub-1 Ghz (15.4 Stack). With DMM it is still possible to easily enable BLE connectivity into the network.
Thanks, Fredrik.
I am not sure star network is comparable as mesh is able to reach points that have no direct connection, but can be reached with hops. I think the self healing ability makes mesh very attractive / robust. Also low power, "friend" and proxy function sounds interesting.
rgds Hansjoerg