This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FCC test BLE Command Needed.



HI

We are using Tiwi-BLE (LSR make) module , whiuch has inside TI RF chip WL1271L. We send out product for FCC testing and we are able to do bluetooth EDR testing but have some issue on BLE testing. pleaser advise here.

For Bluetooth EDR (we used below command)

Step3: Enable Continuous Transmission - FCC Mode)
# Configure Transmitter Parameters

# 0xAA - Modulation Scheme: 0-CW, 1-GFSK, 2-EDR2, 3-EDR3

# 0xBB - Test Pattern: 0-PN9, 1-PN15, 2-Z0Z0, 3-All 1, 4-All 0, 5-F0F0, 6-FF00

# 0xCC - Frequency Index: 0-78

# 0xDD - Power Level: 10(MIN)-15(MAX)

hcitool cmd 0x3F 0x0184 0xAA 0xBB 0xCC 0xDD 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00

BUT TO TEST BLE MODE we need GMSK or BLE modulation . we did not find this in above given command , please provide command to transmit using GMSK / BLE mode to perform the FCC testing.

LSR Module Link :  www.lsr.com/.../330-0087.pdf

processors.wiki.ti.com/.../CC256x_FCC_Testing_Guide