This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: which pins are needed to connect to the CC2650STK DevPack Debug for programming?

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650STK, CC2650

We have an application that is based on the CC2650STK and we wonder if we can get it onto the CC2650MODA.

Obviously the CC2650MODA provides only DIO_0 to DIO_14, so we have to rearrange connected devices.

But the most important question we did not yet find an answer is which pins we need to connect to the CC2650 DevPack-Debug for firmware download.

The CC2650STK has two connectors to the DevPack-Debug and one is for JTAG (TMS,TCK,TDD,TDI, NRESET) and the other is for secondary devices but also includes TDO, TDI and some pins that are in the DIO_15 to DIO_30 range.

And, the CC2560MOD has JTAG TMS, TDO and TDI shared with DIO_5/DIO_6 which are not connected to the JTAG connector of the CC2650STK.

So what is the minimum required connection for a CC2650MOD to a DevPack-Debug to be able to flash firmware?