Hi, I am working on AoA examples in the sdk simplelink_cc2640r2_sdk_2_40_00_32. Master establishes the connection with slave then passive monitors connection and gives us result. Can we get the angle without establishing connection? Can't we use advertisement transmission to get the angle? If we can't do without connection, do I have to disconnect and then connect the new slave device to monitor multiple slave devices(for example 10 devices)?