This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Sensor controller studio example project: Task Control

Part Number: CC2640R2F


Hello,

I was running the task control example project from the SCS. The LED fader task is not exactly performing what it has to do. It is making the LED blink at regular intervals instead of variable intervals based on the onDuration and offDuration parameters for the evhSetupTimer1Trigger(0, onDuration, 2); and evhSetupTimer1Trigger(0, offDuration, 2); procedure calls in Event Handler code. 

I executed the example as it is and did not modify. Am I missing something here? 

Regards,

Swarna