Other Parts Discussed in Thread: CC2564,
Tool/software: Code Composer Studio
The project also will include a CC2564 blue tooth device.
It need only to pair with a microphone and Cell phone.
The microphone will continually transmit voice over blue tooth.
The Cell phone will only send control information and receive status information to display over the blue tooth.
The cell phone will not transmit voice.
I have looked at TIBLUETOOTHSTARC-SDK AND C:\TI\simplelink_cc13x0_sdk_2_40_00_20
TIBLUE TOOTH HAS BLUETOPIA AND Sinplelink has Stack 15.4
This is confusing about which one to use.
I tried to build file in TIBLUETOOTH A3DPDemo_sdk and do not understand how. It looks like I need some Pert what ever that is to build a lib.