Part Number: CC2538-CC2592EM-RD
Other Parts Discussed in Thread: CC2592, CC2538
Hi,
I have a customer who copied the CC2538-CC2592EM-RD in their design but added 3 0ohm resister to do co-layout with on or bypass CC2592.
Now they are seeing the folloiwng issues. Measurements are done by scope and cable loss is 2dB.
1. With CC2592, measure peak power is about -5dBm when target power is set 22dBm by Smart RF Studio.
2. Bypass CC2592, measure peak power is about 4dBm when target power is set 7dBm.
3. Set as RX mode, measure S11 from output of CC2592 to CC2538, S11 are under -10dB, it seems the RF matching is ok.
Hence customer suspect that the CC2592 is not working. Any advise on the issue?
Best Regards,
Dunman Teo