This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/BLE-STACK: I can't to build the simple peripheral example.

Part Number: BLE-STACK

Tool/software: TI-RTOS

I can't to build the simple peripheral example. I am using IAR 7.50.2 and TI BLE Stack SDK 2.02.02.25. I think that there are a problem with the argument variables.
I don't understand what happen. Please any can help me with? Please

Thanks very much. BestRegards

  • Hi,
    The recommended IAR version for that SDK is EWARM-7.80.4. Could you please upgrade and test?
  • Hi J Lindh, Sincerely thanks very much by your answer,


    I have updated the IAR software to IAR 8.32 version (code size limited).


    I have the same problem with IAR 7.50 and IAR 8.32.

    Here I attached a picture of the problem.


    Please, could you tell me if has you some idea of the solution, please?

    Sincerely, Thanks very much.

  • As J Lindh already reply you, each BLE Stack uses specific IAR version and it's recommended to use matched version in release note. For ble_sdk_2_02_02_25, you should use IAR EWARM 7.80.4 and make sure you install ble_sdk_2_02_02_25 under c:\ti to try again.

  • Hi, YiKai Chen

    You're right !!! I've tried with iar 8.32 and it works fine !!!
    I also had another problem, I was using simpleperipheral_app only. It is necessary to use simpleperipheral_app and simpleperipheral_stack in the same workspace and download them. 

    Sincrely thanks very much. Best regards

  • Hi Sir,

    You're right !!! I've tried with iar 8.32 and it works fine !!!
    I also had another problem, I was using simpleperipheral_app only. It is necessary to use simpleperipheral_app and simpleperipheral_stack in the same workspace and download them.



    Sincrely thanks very much. Best regards