Tool/software: TI-RTOS
Dear All,
I"m working with TI RTOS and use the Simple peripheral project,
i have 5 Analog inputs, and need to work with different references as follow:
1. 3 Analog inputs, i need to work with VDDs reference.
2. 2 Analog inputs, i need to work with 1.4v reference.
the only option that i success to do, is to sample all the ADC channels with 4.3v reference
it is possible to use 2 different references at the same time?
if not, how can i change the 4.3V reference to another ADC reference ?
Thanks a lot
Adel