Part Number: CC2564C
I am measuring the RF performance according to the BLE spec
I use below HCI command to measure the peak power and average power. I am using antenna coupling for measurement and the measured power is thus lower because of the antenna coupling lose
HCI command for power measurement: 0x01 0x1E 0x20 0x03 0x00 0x25 0x00
Measured average power: -11.32 dBm
Measurement peak power; -4.24 dBm
According to the BLE spec. Peak power and average power difference should be smaller than 3dB. It seems that for the measurement result, the difference is 7 dB (out of spec) Please comment