This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: PCB antenna for CC2640

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2511,

Hi,

I need to realize a PCB antenna for CC2640R2F, I follow the instruction on Application note AN043, but if I read the PCB characteristic in CC2511_USB_DONGLE_REFERENCE_DESIGN_README_1_3.TXT

I find:

PCB DESCRIPTION:1-2 LAYER PCB 0.25 MM NOMINAL
2-3 LAYER PCB 0.50 MM NOMINAL
3-4 LAYER PCB 0.25 MM NOMINAL
THICKNESS FR4 WITH 35um Cu PER LAYER
Dimensions in mil (0.001 inch)
DOUBLE SIDE SOLDER MASK,
DOUBLE SIDE SILKSCREEN,
8 MIL MIN TRACE WIDTH AND 6 MIL MIN ISOLATION
Dielectric constant for FR4 is 4.5

my PCB is only two layer. In this case what is the distance between top and bottom, 0.25mm or 0.25+0.5+0.25=1mm?

In the application note is written:

To compensate for a thicker/thinner PCB the antenna could be made slightly shorter/longer.

But How do I change the antenna sizes? What is the equations that I have to use?

Thanks.

Best regards.

Giuseppe