Part Number: CC2640R2F
Tool/software: Code Composer Studio
Hi,
I am using CC2640R2F MCU and is connected to a sensor. I want to send the sensor data to an Android application called "Serial Bluetooth Terminal". And i also want to plot that continuous data. So, i have installed CCS 8.3.0 and simplelink_cc2640r2_sdk_2_40_00_32. Tested the examples available in it, they worked perfectly. But those examples are for single application like ADC pin usage shown in "acdsinglechannel" etc. And i tried to create a new project to achieve the aim which involves ADC_init(), GPIO_init(), Display_init() etc. But I got many errors showing missing of header files. I cleared almost but struck at "config.h" file. I found some "config.h" files in simplelink_cc2640r2_sdk_2_40_00_32, but i was unable to find which is suitable one. Actually, I am new to CCS. So, please help me in
1) Creating a new project for Bluetooth usage without any errors.
2) Usage of analog and digital pins
3) How to connect to Android application using Bluetooth.
Please provide any URLs related to these...