Part Number: CC2652R
Tool/software: Code Composer Studio
Hi
I have the very same error like in the post https://e2e.ti.com/support/wireless-connectivity/bluetooth/f/538/t/657834?CC2642R-Problems-with-XDC-Configuro
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ... configuring ble_release.xem4 from package/cfg/ble_release_pem4.cfg ... generating custom ROM library makefile ... TOOLS/subdir_rules.mk:12: recipe for target 'build-1602477985-inproc' failed js: "C:/ti/xdctools_3_51_01_18_core/packages/xdc/cfg/Main.xs", line 48: XDC runtime error: can't find the library 'lib/boot.aem4' specified by package ti.targets.arm.rtsarm. It wasn't found along the path 'C:/ti/simplelink_cc13x2_26x2_sdk_2_40_00_81/source;C:/ti/simplelink_cc13x2_26x2_sdk_2_40_00_81/kernel/tirtos/packages;C:/ti/simplelink_cc13x2_26x2_sdk_2_40_00_81/source/ti/ble5stack;C:/ti/xdctools_3_51_01_18_core/packages;..;'. gmake.exe: *** [package.mak:202: package/cfg/ble_release_pem4.xdl] Error 1 gmake.exe: *** Deleting file 'package/cfg/ble_release_pem4.xdl' gmake.exe: *** [package/cfg/ble_release_pem4.xdl] Deleting file 'package/cfg/ble_release_pem4.h' gmake.exe: *** [package/cfg/ble_release_pem4.xdl] Deleting file 'package/cfg/ble_release_pem4.c' js: "C:/ti/xdctools_3_51_01_18_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted. gmake[1]: *** [build-1602477985-inproc] Error 1 gmake: *** [build-1602477985] Error 2 TOOLS/subdir_rules.mk:9: recipe for target 'build-1602477985' failed gmake: Target 'all' not remade because of errors.
I already tried to start with a fresh example project before and ran into the same error again after adding some files from the SDK-folder into a virtual folder in the project.
It is not possible to revert the error by undoing the changes made. --> same error over and over again.
I don't even find a library called "boot.aem4" only "boot.aem4f" is found somewhere in the SDK folder.
Code Composer Studio Version: 8.3.0.00009
I'm trying to make use of one of the hardware timers (GPT) and this annoying error keeps me from doing what I need to do.
Do you have any suggestions, what can be done to avoid this error?
It generates pretty much work to always start with a fresh project copy of the exampel projects and it just lasts very short!
kind regards
Andreas