This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: Maximum SPI Speed in Master mode without DMA

Part Number: CC2642R

Hello,

I want to transfer image data from an external serial Flash to a small LCD display with a serial interface and an internal framebuffer.

In the technical document SWRS194C the maximum SSI clk cycle time is limited to 12 System Clocks which is only 4 Mbps.

I have successfully tested bitrates of up to 24MHz without DMA and as a SPI Master for both SPI read from the external flash and SPI write to the display framebuffer.

My question is, if the slow 4 Mbps clock is really the guaranteed technical limit under my restrictions (SPI Master, no DMA).

Thank You for Your support!

Kind regards

Oliver