Tool/software: TI C/C++ Compiler
I am working on cc2541 using 1.4.2 stack.I am using SimpleBLEPeripheral.
I want BLE advertise but can not be connectable
// Setup the GAP
VOID GAP_SetParamValue( TGAP_CONN_PAUSE_PERIPHERAL, DEFAULT_CONN_PAUSE_PERIPHERAL );
// Setup the GAP Peripheral Role Profile
{
// For other hardware platforms, device starts advertising upon initialization
uint8 initial_advertising_enable = TRUE;
// By setting this to zero, the device will go into the waiting state after
// being discoverable for 30.72 second, and will not being advertising again
// until the enabler is set back to TRUE
uint16 gapRole_AdvertOffTime = 0;
uint8 enable_update_request = DEFAULT_ENABLE_UPDATE_REQUEST;
uint16 desired_min_interval = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
uint16 desired_max_interval = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
uint16 desired_slave_latency = DEFAULT_DESIRED_SLAVE_LATENCY;
uint16 desired_conn_timeout = DEFAULT_DESIRED_CONN_TIMEOUT;
// Set the GAP Role Parameters
GAPRole_SetParameter( GAPROLE_ADV_NONCONN_ENABLED, sizeof( uint8 ), &initial_advertising_enable );
GAPRole_SetParameter( GAPROLE_ADVERT_OFF_TIME, sizeof( uint16 ), &gapRole_AdvertOffTime );
GAPRole_SetParameter( GAPROLE_SCAN_RSP_DATA, sizeof ( scanRspData ), scanRspData );
GAPRole_SetParameter( GAPROLE_ADVERT_DATA, sizeof( advertData ), advertData );
GAPRole_SetParameter( GAPROLE_PARAM_UPDATE_ENABLE, sizeof( uint8 ), &enable_update_request );
GAPRole_SetParameter( GAPROLE_MIN_CONN_INTERVAL, sizeof( uint16 ), &desired_min_interval );
GAPRole_SetParameter( GAPROLE_MAX_CONN_INTERVAL, sizeof( uint16 ), &desired_max_interval );
GAPRole_SetParameter( GAPROLE_SLAVE_LATENCY, sizeof( uint16 ), &desired_slave_latency );
GAPRole_SetParameter( GAPROLE_TIMEOUT_MULTIPLIER, sizeof( uint16 ), &desired_conn_timeout );
I am using this GAPROLE_ADV_NONCONN_ENABLED to stop connection but device still can be connect. How can i stop connection?