Tool/software: Code Composer Studio
Hello,
When I download the Project Zero example to CCS 8.3, and try to debug it, i get this error:
Cortex_M4_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.903.2)
Cortex_M4_0: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.0.903.2)
I'm currently using Windows 10 and CCS 8.3. This error also happened when I tried to do the same in de CCS Cloud.