Tool/software: Code Composer Studio
I am working with a custom board using the CC1352R to add BLE support to an existing project that currently only runs the sub-1GHz radio. This device will be a peripheral (advertise and wait for "master" to initiate connection).
I have looked through every document I can find and all of the information seems to start from the examples which already have the proper references set up. For example, I can see that the simple_peripheral project has a path variable SRC_BLE_DIR pointing to the ble5stack directory in the SDK and then some 'Other Repositories' based on that variable.
Do I just need to add this variable and (some of) these other repositories manually to my project? Or is there a "wizard" that I am missing to add BLE support to my existing project?
Also, the simple_peripheral application project seems to be dependent on a stack library project. The existing project that I am working with does have a TI-RTOS project on which it is dependent, but will/can it include the BLE stuff or do I need to create another "support" project for BLE?
Is there a guide that I have not found/noticed that provides the steps necessary to add BLE support to an existing project?
Thanks!
.Tim