Hi Team,
I am trying to use the radiotest library 1.11.0 for the production line setup and intend to use the same for caparray(crystal tuning) and gpio control too. Please advice how can i do it?
As of now even if I configure the cap array in my BLE stack and flash that image on my hardware, and then try to measure the frequency offset from the radiotest library then the device still shows the original freqoffset value(thereby indicating that the caparray correction applied through BLE stack in CCFG area has not been taken into consideration).
Secondly, just like smart rf studio it should be allowed to have caparray value correction being applied thorugh radiotestlibrary also.
Thirdly, just because the secondary MAC address is also in CCFG area if the feature to configure this in radiotest library in given then it makes radiotstlibrary a complete software for produciton line.
Please comment.