This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Issue while using er34615 d battery.

Part Number: CC2640R2F

Hello,

I'm using custom made cc2640r2f devices and working on multirole project.

The devices while using D cell 3.6V 19000mAh Lithium Battery ER34615 D battery are not starting and just glowing LED continuously.

But the devices work properly while using cr2477 batteries.

What changes need to be made to the multirole project to make it suitable to run for D type 3.6V battery?

Thanks in advance.

Please advice.