This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: AOA implementation question

Part Number: CC2640R2F

Hi,

I have been testing the RTLS AOA implementation that uses a slave, master and Passive device (with AOA BOOTSTXL multi-antenna board). I had some understanding/clarification questions:

1) Why do we need separate Master and passive devices, Is it purely because of limited RAM and flash memory?

2) If i am just interested in one angle (as my applications requires) and I am not really interested in triangulation or trilateration, can i just use one slave and one master.

3) Why can't I not performs in-phase and quadrature component (IQ) sampling directly on on the master with multiple antennas?

4) In the RTLS toolbox fundamentals document (http://dev.ti.com/tirex/explore/node?node=AKBtFOm6vGAOwDl4OxS.jQ__krol.2c__LATEST), under the section "PC/Central Processing Node", it says that  In a final product, these algorithms may be implemented on an embedded device or even perhaps the RTLS master node. Can you please specify the steps required to achieve that on the master node. Will i still need the passive device?

Thank you.

Regards

Mak

  • Hi Noaman,
    You are correct that i's a memory limitation with the current master implementation that requires a third device (passive). It will not be required in our upcoming official BT5.1 offering. Stay tuned.