Team,
I have a customer working with CC2640R2, and they wanted to verify the following:
Do all three compliant package versions of this chip support real time localization system (RTLS), more specifically the Angle of Arrival component of RTLS? The evaluation board comes with the 7mm x 7mm package and the datasheet suggests that the main difference between the three package sizes is the available GPIOs, but we wanted to ensure that AoA is portable to, say, the DSBGA package of the device. Also, assuming so, do we have any collateral detailing what changes need to be made to port the code from the 7x7 device to the other packages?