Tool/software: Code Composer Studio
Hi RM .
i have some question need to confirm with you :
1. is the CC2640R2F use the PLL to transmitte the ADV and receive the ADV?
2. Can i get the detail of the transiver's spec and also the receiver spec?
3.if the phase error was caused by the PLL transiver at the inital carrier wave@ 2.4G and 250K ?
Leison