Part Number: LAUNCHXL-CC2640R2
Hello,
So, I'm a little confused about how to get scan responses...
There looks to be an error in the code solution though..
if(pAdvRpt->evtType == ADV_RPT_EVT_TYPE_SCAN_RSP) // Shouldn't that be if(pAdvRpt->evtType & ADV_RPT_EVT_TYPE_SCAN_RSP)
I get no scan responses unless I make the change above. Once I make the change, and get scan responses, I can't seem to find simple broadcaster though.
I'm setting it up for active scanning via
GapScan_setPhyParams(SCAN_PRIM_PHY_1M, SCAN_TYPE_ACTIVE, (uint16_t)355, (uint16_t)333);
And I get plenty of scan responses with 0 data length (surrounding devices?) but I can't find the simple broadcaster that is sitting right next to me.
Did I miss something? I'm under the impressin that I just needed to change SCAN_TYPE_PASSIVE to SCAN_TYPE_ACTIVE and I would be good to go.
Thanks,
Jason