Part Number: CC2540
The datasheet mentions device operating voltage range is 2-3.6V. Can we know what is the device behaviour below 2V? (Especially wrt current draw and application code behaviour)
- We have tested our device for this condition and we have seen constant current demand below 1.9V.
- We have a battery powered application and during transmission battery voltage goes below 2V.
- We are trying to understand, what time period of a low voltage pulse can trigger Latch condition?
- Is there a way to prevent a device from going into this condition? (Preferably Software Solution)
Also, there is a need to understand Chip to Chip variations of CC2540, since we are using it in a production environment we need to check the reliability of the device. What kind of Data TI can provide for this?