This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: CC2640R2F: Scanning beacon during connection over BLE 4

Part Number: CC2640R2F

Hello,

I have a query that can the cc2640r2f device Scans for any non-connectable beacon packet during connection mode.

To elaborate the problem, lets take a example, the cc2640R2F is connected over BLE 4.1/ 4.2 with a smart-phone and exchanging some data. At that same stage, if I also want to receive beacon on the cc2640R2F from some other device. Is it possible to have such implementation or is there any example code which can be referred for this problem. I am presently using the host test example for BLE 5 in my application.

Regards

Prateek