This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: Can sensor controller provide extra high performance PWM outputs?

Part Number: CC2652R

Hi team,

My customer is elevating CC2652R and he has a question about sensor controller. need your help!

He uses 3 of 16-bit timer to do other functions but he needs total 8 16-bit PWM outputs. That means there should be other 3 PWM outputs.

PWM cycle: 9ms~18ms;

High voltage duration: 500us~2500us;

error requirement: ±0.5us.

By the way, customer already tried to use IO as the PWM outputs, but it cannot meet the error requirements.

Here, we want to know can sensor controller do this job? To provide 3 high performance PWM outputs.

Thank you!

Yuan