Hi,
I have made a board of CC1352P in 2.4GHz freq band configuration. The PA is also configured for 2.4GHz. The TX power on my board is measured as 19.2dbm whereas as per datasheet it should be 19.5dbm. My setup has a micro UFL on board, connected via micro UFL cable which is further connected via SMA cable to Spectrum analyser. Please advice can the joint between these cables can lead to this TX power loss? if not then what coudl be the cause.