Hi,
I it possible to send more than 20 bytes of data over notification using BLE Stack BLE-CC254x-1.4.2.2.
As when i am send 20 Bytes it is working properly but when i am sending 21 bytes data is not coming.
#define SIMPLEPROFILE_CHAR4_LEN 21
VOID memcpy( (void *)arr_rx_uart, "Abhishek Sharmakumar1", SIMPLEPROFILE_CHAR4_LEN );
SimpleProfile_SetParameter( SIMPLEPROFILE_CHAR4, SIMPLEPROFILE_CHAR4_LEN, (void *)arr_rx_uart);
it is working when i am setting #define SIMPLEPROFILE_CHAR4_LEN 20