This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC13X2-26X2-SDK: Connection still drops when limited discoverable period ends

Part Number: SIMPLELINK-CC13X2-26X2-SDK

My original thread was locked, so I'm reposting here.

I'm now using CCS 9.0.1.00004 and updated our project to use the latest simplelink_cc13x2_26x2_sdk_3_10_00_53 SDK.  Unfortunately, the issue still persists.  Limited discoverable mode (GAP_ADV_ENABLE_OPTIONS_USE_DURATION) still crashes the radio if you're connected when the advertising duration timer would end.

See the "Original question" link above for the original details.