This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: BLE 4.2 listing expiration

Part Number: CC2640R2F

Hi team,

at the moment there are 2 Qualified Design Listings for the stacks for CC2640R2F: One for BLE 4.2 stack and one for BLE 5.0 stack. My customer wants to stay with 4.2.

Does this listing expire and If so when would they have to move to 5.0?

Can the BLE 4.2 stack listing for CC2640R2F still be used for product qualification in 2020?

Thank you,

Franz

  • Hi Franz,
    Please refer to this thread: e2e.ti.com/.../2973072

    The CC2640R2 v4.2 listing expire June 22 (2019). If they create their End-Product listing before this date, it will be valid for the product lifetime. If they miss this date, they will have to migrate to SDKv3.20 which is anticipated in July with a new updated QDID. The new QDID will be Bluetooth 5.1 even though the feature set is Bluetooth 4.2 (All Bluetooth 5 features are optional).