This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640R2F: SimpleLink SDK Simple Peripheral Example Flash code size

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2642R,

Tool/software: Code Composer Studio

I'm using the example simple_peripheral from the simplelink_cc2640r2_sdk_3_10_00_15 sdk version and just noticed the amount of flash memory use. I guess the "ongoing" update mentionned here (https://e2e.ti.com/support/wireless-connectivity/bluetooth/f/538/t/715504) is not yet implemented. The stack now uses 92% of the whole flash memory which is useless as a starting point for a custom application. Do you have an update on this point?

Thank you