Part Number: CC2564
Hello
I am currently designing a system where several digital audio sources will be mixed together in a codec/DSP.
To avoid the need for sample rate conversion we want to keep all digital audio streams at even multiples of 8 kHz (that is 8, 16 or 48 kHz)
When CC2564 works as an assisted A2DP sink, can we configure it in such a way that the PCM always uses 48 kHz, or must our system be prepared to handle 44.1 kHz sample rate as well?
BR
Joakim