This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODA: Questions for A2DP

Part Number: CC2564MODA

Hi,

My customer is planning to use A2DP with CC2564MODA.
They have below questions. Please answer them.

Q1) Are there any functional difference between Bluetooth Master and Slave?
I think device search is performed only by Master. Advertisement is only Slave side.
What else? For example, either can be sink or source?

Q2) A2DP data includes volume information, correct?
(There is no separated “volume parameter”?)

Q3) If answer to Q2 is Yes, volume control is done by source device, right?

Q4) Is it possible to determine below status from A2DP data?
4-1 : play back on
4-2 : play pause
4-3 : volume zero
4-4 : mute

Q5) If answer to Q4 is No, does AVRCP profile support them?

Thanks and regards,
Koichiro Tashiro