Other Parts Discussed in Thread: UNIFLASH, ,
Hello,
I have a CC2650 LaunchPad v1.2 with a CC2650F128 revD (2.2) chip. I'd like to use it as a packet sniffer, but it is not recognized by Smart RF Sniffer Agent. I used Uniflash to flash the correct sniffer_fw.hex, and this process proceeded to a successful completion. I installed Wireshark (2.6.9 last release prior to 3.0) and then Smart RFPacket Sniffer 2. I allowed the add-ins to be included as part of the installation as instructed. When I open the snffer agent it doesn't detect the device. The screen is shown below.
Do I have incompatible hardware? Is there a way to tell sniffer agent where to find the hardware - COM17, etc.? Any help on this would be appreciated.
Patrick