Part Number: CC2564MODA
Tool/software: Linux
Hi Team,
We are using CC2564MODA which is interface through UART and connected to PC,
We need to put device in sleep mode according to this documment https://www.mouser.it/pdfdocs/bluetooth-Core-v50.pdf | at Part D page 2462 .
in this document for sleep command payload value is MSB 0X78 and LSB 0X07, 0X7807 binary is 0111 1000 0000 0111
ocf is 10 bit from LSB : 00 0000 0111 (0X007)
ogf is remaining 6 bit : 0111 10 (0X1e)
using HCI command we sent sleep command as below
hcitool -i hci0 cmd 0x1e 0x07
< HCI Command: ogf 0x1e, ocf 0x0007, plen 0
> HCI Event: 0x0e plen 4
01 07 78 01
as per the HCI command if it is return 00 means Command succeeded. and 01 - FF means Command failed.
is this proper way to set the device in sleep?
if it is not let us know, how we can put device in sleep mode using sleep message (0X7807)?