Hi ,
We have two models of CC2642 chips, please see the following photos, let's call the first photo as chip#1 and the second photo as chip#2.
About chip#1, it can run and boot for SDK's example(driver & ble5stack).
About chip#2, it can't boot the project_zero example without JTAG debugging, others example can be boot.(we have downloaded BIM image). In the un-bootable
state, we found that the CC2642 doesn't output a 48MHz clock. Do you have any suggestion to us?
Thanks.
BR
Trevor