Other Parts Discussed in Thread: LMP91000, CC2541, , CC2642R, CC2640R2F
Hi Team,
I am planing to use CC2540/ CC2541 for gas sensing application and I understood How to interface could gas sensor along with LMP91000.
Could you please help me understand CC2540/ CC2541 (BEL + SOC), will supports below my Features.
|
Features |
YES/ NO |
|
External SD card ( Memory) |
|
|
TCP/Ip |
|
|
Bluetooth( BLE) |
|
|
Additional board level communication ( other than Jtag, May be USB port – not for the user ,to be used by service and manufacturing) |
|
|
Support external 4G Modem |
|
|
Additional data Transmission protocols ( HTTPS,MQTT –Future proofing) |
|
|
Supports Encryption |
|
|
Encrypted Transmission |
|
|
Resources to add additional features in the future ( DNP3 Level 3, MQTT etc..) |
|
|
Industrial grade ( -40 to 70 degrees) |
|
|
LCD |
|
|
Diagnostics (hardware and Firmware level) |
|
|
Additional inputs ( Analog ) |
|
|
Additional/optional outputs ( 4-20 , Modbus) |
|
Thanks
Abhay