Part Number: CC2564MODA
Other Parts Discussed in Thread: CC2564, CC256XB-BT-SP
Hi,
I am working on an Audio Bluetooth product using a CC2564MODA, which is to be used in industrial environments with signal strength restrictions. The need is to limit the Bluetooth signal to +4dBm. The Bluetooth specification calls that a Class 2 device whereas the CC2564 is ranked as a Class 1.5 in the datasheet (so it can issue a +10dBm signal).
If I did not misunderstand documentations, the signal strength has to be set during the service pack upload. I tried to generate my own CC256XB.h file to be upload but then, I have not the material to test signal strength.
Could you provide me a CC256XB.h file containing the CC256XB-BT-SP v1.7 + AVPR Patch + Class 2 limited signal strength?
Thanks in advance for any help.
Regards,
Alain