This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: Pairing mode doesn't work

Part Number: LAUNCHXL-CC26X2R1


Hi All,

I am using LAUNCHXL-CC26X2R1 board. I am trying to change the pairing mode in both peripheral and central project examples, but I figured out no matter  which piring mode I choose, central always can connect to the peripheral! I even change the peripheral pair mode to GAPBOND_PAIRING_MODE_NO_PAIRING but still central can connect!

I need to change the pair mode to Numeric Comparison so as per the documentation I expect that "both devices display a 6-digit code. Each device must then indicate, through a button press or some other Yes-No input, whether the codes match" but doesn't work for me, am I missing something? 

Thanks,